Solution
Sanding Machine Force Monitoring
A machining company that sells large sanding machines needs a force system to measure the z-axis of their machines.

3AXX 3-Axis Force Load Cell
BSC4A Multi-Channel Bridge Amplifier
Customer’s controls
Customer’s sanding machine being tested
The 3AXX 3-Axis Load Cell is installed between the sanding machine’s sanding block and the head of the machine that will be putting pressure on the material being sanded.
When connected to the BSC4A Multi-Channel Bridge Amplifier, it will convert the mv/V signal from the 3-Axis load cell to a signal (voltage or mA) which can communicate directly with the customer’s control system.